How to use the rtcs shell on ethernet instead of on a serial port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the rtcs shell on ethernet instead of on a serial port

Jump to solution
1,070 Views
jpderyck
Contributor II

The rtcs shell demo run on a serial port, how to run it on ethernet ?

It was possible on the security_telnet sample which was available with mqx version before 4.0,

I use the mqx 4.1 in wich this demo was removed

best regards

JP

Labels (1)
0 Kudos
Reply
1 Solution
909 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Paul,

The shell is targeted to work with the serial (CDC) interface. But you can also start a telnet session to take contro remotely of the Shell. Please take a look to the _README.txt file in C:\Freescale\Freescale_MQX_4_x\rtcs\examples\shell

Best regards,

Carlos

View solution in original post

0 Kudos
Reply
1 Reply
910 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Paul,

The shell is targeted to work with the serial (CDC) interface. But you can also start a telnet session to take contro remotely of the Shell. Please take a look to the _README.txt file in C:\Freescale\Freescale_MQX_4_x\rtcs\examples\shell

Best regards,

Carlos

0 Kudos
Reply