I made a document with some print screens and it is attached. The print screens don't paste.
Referring to the "How to Change Default Clock Setting in Kinetis BSPs" I completed this procedure summarized in the attachment called: Custom Clock
I basically end up with errors:
mingw32-make: *** [Peripheral IO Drivers/usb_dcc/int/usb_dcd_int_kn_c.obj] Error 1 bsp_Console_MK60FX512VLQ12 C/C++ Problem
mingw32-make: *** [Peripheral IO Drivers/usb_dcc/polled/usb_dcd_pol_kn_c.obj] Error 1 bsp_Console_MK60FX512VLQ12 C/C++ Problem
mingw32-make: *** [Peripheral IO Drivers/usb_dcc/usb_dcd_mk60_c.obj] Error 1 bsp_Console_MK60FX512VLQ12 C/C++ Problem
mingw32-make: *** [Sources/Events_c.obj] Error 1 bsp_Console_MK60FX512VLQ12 C/C++ Problem
I already opened a service request on this issue number: 1-1054023221
Unfortunately, they couldn't duplicate these errors doing exactly what I am doing. I have tried this on two computers and get the same results.
My questions are:
Has anyone else seen this?
Is there a solution?
I think I must be doing something dumb when following the procedure.
The second attached document is what the service rep. sent me called:
Solved! Go to Solution.
Hey thanks for pointing out the proper way to use the console window!
Knowing this...
C:/Freescale/CW MCU v10.4/MCU/ARM_Tools/Command_Line_Tools/mwccarm|Compiler|Error
(C:\Freescale\Freescale_MQX_4_0\mqx\build\cw10\bsp_Console_MK60FX512VLQ12\Generated_Code\Cpu.c|1207|15|19|55109|19)
= SIM_SCGC4 |= SIM_SCGC4_LLWU_MASK;
>undefined identifier 'SIM_SCGC4_LLWU_MASK'
I was able to find 'SIM_SCGC4_LLWU_MASK' was undefined in cpu.c even though it included "IO_Map.h" which defined 'SIM_SCGC4_LLWU_MASK' as 0x10000000u. Not really sure what the problem was but I took 0x10000000u and put it in place of 'SIM_SCGC4_LLWU_MASK' in cpu.c and it compiled fine.
I am not sure this is the correct answer, but it fixed the compile error.
I've run into this on a project here and so dug into it a bit.
It seems that we're using a psp customized from one that has an out-of-date MK60f15.h, which #defines the memory model guard macro MCU_MK60F12 and thus prevents the IO_Map.h from declaring it. The newer psp (included with CW 10.5) seems to fix it.
The relevant parts of the older MK60f15.h header are:
** Reference manual: K60P144M150SF3RM, Rev. 1, Oct 2011
** Version: rev. 1.3, 2011-11-18
     ...
/* SCGC4 Bit Fields */
#define SIM_SCGC4_EWM_MASK 0x2u
#define SIM_SCGC4_EWM_SHIFT 1
....
#define SIM_SCGC4_VREF_MASK 0x100000u
#define SIM_SCGC4_VREF_SHIFT 20
/* SCGC5 Bit Fields */
The relevant parts of IO_Map.h are:
** Reference manual: K60P144M150SF3RM, Rev. 2, Dec 2011
** Version: rev. 1.9, 2013-06-24
...
    /* SCGC4 Bit Fields */
    #define SIM_SCGC4_EWM_MASK                       0x2u
    #define SIM_SCGC4_EWM_SHIFT                      1
    ...
    #define SIM_SCGC4_VREF_MASK                      0x100000u
    #define SIM_SCGC4_VREF_SHIFT                     20
     #define SIM_SCGC4_LLWU_MASK                      0x10000000u
    #define SIM_SCGC4_LLWU_SHIFT                     28
    /* SCGC5 Bit Fields */
(Forgot to Finish This)
The second attached document is what the service rep. sent me called:
In order to reproduce your issue.pdf
Hello Colin Dawson,
could you please explain me why do you share problems output , not the console? Does those error say anything to you ? They are meaningless to me. Share a console output the next time.
Could you share yours generated project?
Regards,
c0170
Hey thanks for pointing out the proper way to use the console window!
Knowing this...
C:/Freescale/CW MCU v10.4/MCU/ARM_Tools/Command_Line_Tools/mwccarm|Compiler|Error
(C:\Freescale\Freescale_MQX_4_0\mqx\build\cw10\bsp_Console_MK60FX512VLQ12\Generated_Code\Cpu.c|1207|15|19|55109|19)
= SIM_SCGC4 |= SIM_SCGC4_LLWU_MASK;
>undefined identifier 'SIM_SCGC4_LLWU_MASK'
I was able to find 'SIM_SCGC4_LLWU_MASK' was undefined in cpu.c even though it included "IO_Map.h" which defined 'SIM_SCGC4_LLWU_MASK' as 0x10000000u. Not really sure what the problem was but I took 0x10000000u and put it in place of 'SIM_SCGC4_LLWU_MASK' in cpu.c and it compiled fine.
I am not sure this is the correct answer, but it fixed the compile error.
Hello,
I had read you previous message therefore I was going to point to that LLWU_MASK. I am glad that you have solved it. I always keep the console opened while coding, helps a lot. Problem tab is useless for me the most of time :smileywink:
Regards,
c1070
Here is my console information...
C:/Freescale/CW MCU v10.4/MCU/ARM_Tools/Command_Line_Tools/mwccarm|Compiler|Error
(C:\Freescale\Freescale_MQX_4_0\mqx\build\cw10\bsp_Console_MK60FX512VLQ12\Generated_Code\Cpu.c|1207|15|19|55109|19)
= SIM_SCGC4 |= SIM_SCGC4_LLWU_MASK;
>undefined identifier 'SIM_SCGC4_LLWU_MASK'
'Invoking: ARM Compiler'
'Finished building: C:/Freescale/Freescale_MQX_4_0/mqx/source/io/debug/iodebug.c'
"C:/Freescale/CW MCU v10.4/MCU/ARM_Tools/Command_Line_Tools/mwccarm" -gccinc @@"Generated_Code/GPIO1.args" -o "Generated_Code/GPIO1_c.obj" -c "../Generated_Code/GPIO1.c" -MD -gccdep
'Invoking: ARM Compiler'
'Finished building: C:/Freescale/Freescale_MQX_4_0/mqx/source/io/cm/cm.c'
"C:/Freescale/CW MCU v10.4/MCU/ARM_Tools/Command_Line_Tools/mwccarm" -gccinc @@"Generated_Code/MQX1.args" -o "Generated_Code/MQX1_c.obj" -c "../Generated_Code/MQX1.c" -MD -gccdep
' '
' '
'Finished building: ../Generated_Code/GPIO1.c'
' '
'Finished building: ../Generated_Code/MQX1.c'
' '
'Finished building: C:/Freescale/Freescale_MQX_4_0/mqx/source/io/debug/iodebug_asm.S'
' '
Errors caused tool to abort.
mingw32-make: *** [Generated_Code/Cpu_c.obj] Error 1
mingw32-make: *** Waiting for unfinished jobs....