Does MQX 4.0 support configuring a UART for 7 data bits, odd parity?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MQX 4.0 support configuring a UART for 7 data bits, odd parity?

Jump to solution
2,395 Views
gorakk
Contributor IV

Has anyone been able to configure for 7 data bits odd parity?

7 data bits, odd parity is required for operation with some existing equipment.

After reading through the RM and reading some answers on this site I thought I could use IO_IOCTL_SERIAL_SET_DATA_BITS to set for 8-bit mode (for 7 data bits and 1 parity bit)  and IO_IOCTL_SERIAL_SET_PARITY to set parity to IO_SERIAL_PARITY_ODD.  But - when trying to communicate with a port set like this, a PC terminal program shows garbage characters.

Stepping through the MQX code shows that in _kuart_polled_ioctl() - setting ODD parity also sets 9-bit mode: sci_ptr->C1 |= UART_C1_M_MASK;

The IO_IOCTL_SERIAL_SET_PARITY case from _kuart_polled_ioctl():

      case IO_IOCTL_SERIAL_SET_PARITY:

         switch (*param_ptr) {

            case IO_SERIAL_PARITY_NONE:

               /* disable parity only if enabled (once) */

               if (sci_ptr->C1 & UART_C1_PE_MASK)

               {

                  sci_ptr->C1 &= (~ (UART_C1_PE_MASK | UART_C1_PT_MASK));

               

                  /* disable parity bit */

                  if (sci_ptr->C4 & UART_C4_M10_MASK)

                  {

                     sci_ptr->C4 &= (~ UART_C4_M10_MASK);

                  }

                  else

                  {

                     sci_ptr->C1 &= (~ UART_C1_M_MASK);

                  }

               }

               break;

            case IO_SERIAL_PARITY_ODD:

               /* can't enable parity in 2 stop bits mode */

               if (IO_SERIAL_STOP_BITS_1 != (io_info_ptr->FLAGS & IO_SERIAL_STOP_BITS_1))

               {

                  return MQX_INVALID_CONFIGURATION;

               }

               /* if parity already enabled, just set the requested one */

               if (sci_ptr->C1 & UART_C1_PE_MASK)

               {

                  sci_ptr->C1 |= UART_C1_PT_MASK;

               }

               else

               {

                  /* enable odd parity */

                  sci_ptr->C1 |= (UART_C1_PE_MASK | UART_C1_PT_MASK);

               

                  /* enable parity bit */

                  if (sci_ptr->C1 & UART_C1_M_MASK)

                  {

                     sci_ptr->C4 |= UART_C4_M10_MASK;

                  }

                  else

                  {

                     sci_ptr->C4 &= (~ UART_C4_M10_MASK);

                     sci_ptr->C1 |= UART_C1_M_MASK;

                  }

               }

               break;

            case IO_SERIAL_PARITY_EVEN:

                /* can't enable parity in 2 stop bits mode */

               if (IO_SERIAL_STOP_BITS_1 != (io_info_ptr->FLAGS & IO_SERIAL_STOP_BITS_1))

               {

                  return MQX_INVALID_CONFIGURATION;

               }

            

               /* if parity already enabled, just set the requested one */

               if (sci_ptr->C1 & UART_C1_PE_MASK)

               {

                  sci_ptr->C1 &= (~ UART_C1_PT_MASK);

               }

               else

               {

                  /* enable even parity */

                  sci_ptr->C1 |= UART_C1_PE_MASK;

                  sci_ptr->C1 &= (~ UART_C1_PT_MASK);

               

                  /* enable parity bit */

                  if (sci_ptr->C1 & UART_C1_M_MASK)

                  {

                     sci_ptr->C4 |= UART_C4_M10_MASK;

                  }

                  else

                  {

                     sci_ptr->C4 &= (~ UART_C4_M10_MASK);

                     sci_ptr->C1 |= UART_C1_M_MASK;

                  }

               }

               break;

            default:

               return MQX_INVALID_PARAMETER;

         }

         break;

/* Message was edited by: Martin Kojtal */

Use C++ highlighter ( https://community.freescale.com/docs/DOC-94815). Thank you, c0170

0 Kudos
Reply
1 Solution
1,790 Views
c0170
Senior Contributor III

Hello Allen Johnson-Weltzin,

have you check what configurations does your kinetis support?

I checked code and RM. Both seem to support 8 and 9 bit data bits plus parity. Not 7 data bits and parity. (RM - 51.4.4 Data format (non ISO-7816)  from Kinetis k60).

Regards,

c0170

View solution in original post

0 Kudos
Reply
2 Replies
1,791 Views
c0170
Senior Contributor III

Hello Allen Johnson-Weltzin,

have you check what configurations does your kinetis support?

I checked code and RM. Both seem to support 8 and 9 bit data bits plus parity. Not 7 data bits and parity. (RM - 51.4.4 Data format (non ISO-7816)  from Kinetis k60).

Regards,

c0170

0 Kudos
Reply
1,790 Views
gorakk
Contributor IV

Thanks for the help, Martin.

What I wound up doing is, when 7-even or 7-odd is needed, set for 8-bit mode and then manually set the most significant bit of the character being transmitted.  For characters being received in 7-even or 7-odd I simply clear the most significant bit.

Also, thanks for the tip on code formatting in posts.

Regards,

Allen

0 Kudos
Reply