Concurrent use of MQX3.7 and MQX3.8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Concurrent use of MQX3.7 and MQX3.8

跳至解决方案
985 次查看
MarkP_
Contributor V

Hi,

made one project with MQX3.7 and CW10.1. Project almost finished, some support still needed.

Don't like to upgrade this project to MQX3.8.

 

Now starting a new project, want to use MQX3.8 and CW10.2.

Is it possible to install MQX3.8 and still the older MQX3.7 stays operable?

Is CW10.2 compatible with MQX3.7?

 

At least this need to be changed when switching MQX3.7 <-> MQX3.8:

MQX_PATH=C:\Program_Files\Freescale\Freescale MQX 3.7

Is there any other MQX-settings in registry which need to be changed?

 

~Mark

 

 

0 项奖励
回复
1 解答
765 次查看
petr_uhlir
NXP Employee
NXP Employee

Mark,

its not a problem to have installed different versions of MQX an CodeWarrior (and other) compilers. The only thing you have to do is to manualy install CodeWarrior extensions (TAD, RTOS adaptor, Wizards,..)

from "src\tools\codewarrior_extensions\CW MCU v10.2\"

 

You will be able to open existing projects created for MQX 3.7 & CW 10.1, modify, debug,...etc.

The only thing which is not supported in 10.2 is new project wizard for MQX 3.7

 

Petr

在原帖中查看解决方案

0 项奖励
回复
1 回复
766 次查看
petr_uhlir
NXP Employee
NXP Employee

Mark,

its not a problem to have installed different versions of MQX an CodeWarrior (and other) compilers. The only thing you have to do is to manualy install CodeWarrior extensions (TAD, RTOS adaptor, Wizards,..)

from "src\tools\codewarrior_extensions\CW MCU v10.2\"

 

You will be able to open existing projects created for MQX 3.7 & CW 10.1, modify, debug,...etc.

The only thing which is not supported in 10.2 is new project wizard for MQX 3.7

 

Petr

0 项奖励
回复