CodeWarrior 10.x & MQX Documentation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 10.x & MQX Documentation?

Jump to solution
2,033 Views
BenG
Contributor III

I normally use IAR Embedded Workbench, but I want to experiment with using Code Warrior. I'm not overly familiar with the Eclipse IDE/Interface but I can do some basic development with it.

 

Is there any documentation available which covers using MQX 3.x with CodeWarrior 10.x?

 

I can find documentation for  MQX 3.8 and CW 10.x, but no documentation that covers both together. The MQX documentation that refers to CodeWarrior refers to the "classic" version (i.e. 6.x/7.x) (e.g. AN3905) which is obviously significantly different from the Eclipse interface used in 10.x,

 

 

0 Kudos
Reply
1 Solution
1,718 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

 

Have you seen this doc? It is part of MQX3.7 docs

 

Best Regards,

View solution in original post

0 Kudos
Reply
2 Replies
1,719 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

 

Have you seen this doc? It is part of MQX3.7 docs

 

Best Regards,

0 Kudos
Reply
1,718 Views
BenG
Contributor III

Cheers Luis,

 

That's exactly what I was after.

 

Thanks

0 Kudos
Reply