CodeWarrior 10.x & MQX Documentation?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 10.x & MQX Documentation?

ソリューションへジャンプ
2,029件の閲覧回数
BenG
Contributor III

I normally use IAR Embedded Workbench, but I want to experiment with using Code Warrior. I'm not overly familiar with the Eclipse IDE/Interface but I can do some basic development with it.

 

Is there any documentation available which covers using MQX 3.x with CodeWarrior 10.x?

 

I can find documentation for  MQX 3.8 and CW 10.x, but no documentation that covers both together. The MQX documentation that refers to CodeWarrior refers to the "classic" version (i.e. 6.x/7.x) (e.g. AN3905) which is obviously significantly different from the Eclipse interface used in 10.x,

 

 

0 件の賞賛
返信
1 解決策
1,714件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

 

Have you seen this doc? It is part of MQX3.7 docs

 

Best Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,715件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

 

Have you seen this doc? It is part of MQX3.7 docs

 

Best Regards,

0 件の賞賛
返信
1,714件の閲覧回数
BenG
Contributor III

Cheers Luis,

 

That's exactly what I was after.

 

Thanks

0 件の賞賛
返信