BSP Clone Wizard not launching

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BSP Clone Wizard not launching

跳至解决方案
5,060 次查看
bonzo
NXP Employee
NXP Employee

Clone Wizard does launch on my Win7 64-bit PC for any version of MQX4.0 or 4.1.

I get the following error:

pastedImage_9.png

Here is he version of Java I am running:

pastedImage_10.png

0 项奖励
回复
1 解答
4,752 次查看
bonzo
NXP Employee
NXP Employee

David,

I installed the 32-bit version of Java, and now it appears to work.

Brad

在原帖中查看解决方案

3 回复数
4,752 次查看
DavidS
NXP Employee
NXP Employee

Hi Brad,

Very weird.  The default Java on my Windows 7 64-bit was Java 32-bit.  I downloaded and installed Java 64-bit and it now is the default Java engine and it works with my BSPCloningWizard.

You might try adding the path to the javaw into your Environmental variable PATH to see if that help.

Otherwise I can only suggest un-installing both Java and MQX, reboot and re-install to see if it fixes the path issue.

Sorry I cannot reproduce the issue.

Regards,

David

4,753 次查看
bonzo
NXP Employee
NXP Employee

David,

I installed the 32-bit version of Java, and now it appears to work.

Brad

4,655 次查看
mmalagon
Contributor II

Here I am 7 years later benefiting from this solution.

Thanks!

0 项奖励
回复