BSP Clone Wizard not launching

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP Clone Wizard not launching

Jump to solution
5,127 Views
bonzo
NXP Employee
NXP Employee

Clone Wizard does launch on my Win7 64-bit PC for any version of MQX4.0 or 4.1.

I get the following error:

pastedImage_9.png

Here is he version of Java I am running:

pastedImage_10.png

0 Kudos
Reply
1 Solution
4,819 Views
bonzo
NXP Employee
NXP Employee

David,

I installed the 32-bit version of Java, and now it appears to work.

Brad

View solution in original post

3 Replies
4,819 Views
DavidS
NXP Employee
NXP Employee

Hi Brad,

Very weird.  The default Java on my Windows 7 64-bit was Java 32-bit.  I downloaded and installed Java 64-bit and it now is the default Java engine and it works with my BSPCloningWizard.

You might try adding the path to the javaw into your Environmental variable PATH to see if that help.

Otherwise I can only suggest un-installing both Java and MQX, reboot and re-install to see if it fixes the path issue.

Sorry I cannot reproduce the issue.

Regards,

David

4,820 Views
bonzo
NXP Employee
NXP Employee

David,

I installed the 32-bit version of Java, and now it appears to work.

Brad

4,722 Views
mmalagon
Contributor II

Here I am 7 years later benefiting from this solution.

Thanks!

0 Kudos
Reply