BLE OSAL Abstract Layer create task

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLE OSAL Abstract Layer create task

Jump to solution
1,874 Views
mkrishna
Contributor I

Hi Team,

     Our Application is QN9080 BLE based Control System with Battery power.

    can you please suggest or help with the below queries.

     1. Need a confirmation to use a Baremetal or FreeRTOS BLE Abstract layer for our Application.

     2. if we use a BareMetal based Abstract layer, then please provide the example program for how to create a task.

 

Thanks,

Krishna  

0 Kudos
Reply
1 Solution
1,846 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi mkrishna, I hope you're doing well!

 

Depending on the needs of your application, either one of the available abstraction layers may be useful to use for development.

 

Could you please take a look at the following community document for help with creating a new task using the OS Abstraction layers on the BLE Stack for QN9080?

Using the QN908x FreeRTOS BLE Abstraction Layer St... - NXP Community

 

Please let me know if you need any more information.

Best regards,
Sebastián

View solution in original post

0 Kudos
Reply
1 Reply
1,847 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi mkrishna, I hope you're doing well!

 

Depending on the needs of your application, either one of the available abstraction layers may be useful to use for development.

 

Could you please take a look at the following community document for help with creating a new task using the OS Abstraction layers on the BLE Stack for QN9080?

Using the QN908x FreeRTOS BLE Abstraction Layer St... - NXP Community

 

Please let me know if you need any more information.

Best regards,
Sebastián

0 Kudos
Reply