How to properly configure several FLEXCAN message buffers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to properly configure several FLEXCAN message buffers

1,414件の閲覧回数
stefpopa
Contributor I

Hello,

I  am running a modified flexcan_interrupt_transfer.c example on an iMXQM6 processor. I am using CAN FD and only care about receiving messages from a PCAN-View probe which I use for testing. 

From the PCAN-View probe, I am sending several messages with a cycle time of 1ms to the same ID which as in the example is set by default to 0x123h. 

I observed that some of the messages were lost, so I configured all the message buffers from 0x01 to 0x14 to receive data from the same ID. However, the messages are still being lost and it seems that only the first message (with the highest priority) is used. 

I checked that bit 16 (IRMQ) from the MCR register is set and I configured the Rx Mb Gobal Mask:FLEXCAN_SetRxMbGlobalMask(EXAMPLE_CAN, FLEXCAN_RX_MB_STD_MASK(rxIdentifier, 0, 0)); but with no success.

Is there something else that I am missing?

Thank you in advance for your support!

-Stefan

0 件の賞賛
返信
1 返信

1,341件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

If my understanding is correct you have your board as A node in the example, if that is the case please make sure that your modifications are working correctly for this node.

Would be great if you could share the modifications to the example.

Best regards,
Aldo.

0 件の賞賛
返信