AN4368 is based on which MQX version?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN4368 is based on which MQX version?

ソリューションへジャンプ
1,557件の閲覧回数
Wanderer
Contributor II

AN4368 works great but I would like to reuse the MQX files in my application.  Which version of MQX is this based on?  I noticed that many of the files are much smaller than MQX 3.6.

 

Thanks, gj

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,321件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi gj,

The AN4368 is a baremetal USB stack independent of MQX and its USB stack.

The AN4368 can be used to erase/program flash application that is MQX or baremetal.

Correct that the baremetal codebase is smaller than equivalent MQX implementation.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,322件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi gj,

The AN4368 is a baremetal USB stack independent of MQX and its USB stack.

The AN4368 can be used to erase/program flash application that is MQX or baremetal.

Correct that the baremetal codebase is smaller than equivalent MQX implementation.

Regards,

David

0 件の賞賛
返信