AN4368 is based on which MQX version?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

AN4368 is based on which MQX version?

跳至解决方案
608 次查看
Wanderer
Contributor II

AN4368 works great but I would like to reuse the MQX files in my application.  Which version of MQX is this based on?  I noticed that many of the files are much smaller than MQX 3.6.

 

Thanks, gj

标签 (1)
标记 (1)
0 项奖励
1 解答
372 次查看
DavidS
NXP Employee
NXP Employee

Hi gj,

The AN4368 is a baremetal USB stack independent of MQX and its USB stack.

The AN4368 can be used to erase/program flash application that is MQX or baremetal.

Correct that the baremetal codebase is smaller than equivalent MQX implementation.

Regards,

David

在原帖中查看解决方案

0 项奖励
1 回复
373 次查看
DavidS
NXP Employee
NXP Employee

Hi gj,

The AN4368 is a baremetal USB stack independent of MQX and its USB stack.

The AN4368 can be used to erase/program flash application that is MQX or baremetal.

Correct that the baremetal codebase is smaller than equivalent MQX implementation.

Regards,

David

0 项奖励