AN4368 is based on which MQX version?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN4368 is based on which MQX version?

Jump to solution
609 Views
Wanderer
Contributor II

AN4368 works great but I would like to reuse the MQX files in my application.  Which version of MQX is this based on?  I noticed that many of the files are much smaller than MQX 3.6.

 

Thanks, gj

Labels (1)
Tags (1)
0 Kudos
1 Solution
373 Views
DavidS
NXP Employee
NXP Employee

Hi gj,

The AN4368 is a baremetal USB stack independent of MQX and its USB stack.

The AN4368 can be used to erase/program flash application that is MQX or baremetal.

Correct that the baremetal codebase is smaller than equivalent MQX implementation.

Regards,

David

View solution in original post

0 Kudos
1 Reply
374 Views
DavidS
NXP Employee
NXP Employee

Hi gj,

The AN4368 is a baremetal USB stack independent of MQX and its USB stack.

The AN4368 can be used to erase/program flash application that is MQX or baremetal.

Correct that the baremetal codebase is smaller than equivalent MQX implementation.

Regards,

David

0 Kudos