MQX软件解决方案知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX Software Solutions Knowledge Base

讨论

排序依据:
Hi all, I want to share this document that describes steps to create a new driver using MQX 4.1 and CW 10.6.  I used the Null-Device Driver,  the null device driver provides an I/O device that functions as a device driver but does not perform any work. I hope it helps. Regards Sol
查看全文
Que tal, Este documento es para toda persona que comienzan a trabajar con MQX . El documento describe como crear una tarea y como usar el driver LWGPIO. Esta escrito en español pensando en nuestros clientes de habla hispana. Saludos Sol
查看全文
MQX includes a great demo for the web server in \<MQX_Path>\demo\web_hvac.  The web pages in this demo show how MQX can serve up data through the web server, and dynamically update the web page, for example the thermostat hvac properties are updated every second.  Also, the user can use a web page form to submit data to the server and update the application, like changing the temperature set point.  This is done with HTML forms, javascript, and CGI running in the MQX application. However, the web_pages directory in the web_hvac demo is missing the actual source files for the web pages.  Starting with MQX v4.0.2, they disappeared from the MQX release.  And since then, the web server APIs and CGI functionality has changed.  Posted here is the web_page directory for web_hvac, including the source code for the web pages.
查看全文
The Freescale MQX™ RTOS for Kinetis SDK FRDM-KL43Z Freescale Freedom Platform is now available on the www.freescale.com ·         Release Files             # Name Description 1                                   Freescale_MQX_KSDK_1.0.0-KL43Z.exe Windows installer. Freescale MQX™ RTOS software   components fully pre-integrated with the Kinetis SDK. Includes the MQX   kernel, USB host and device stacks, MFS file system, and example   applications. Does not require prior installation of Kinetis SDK. 2                                   Freescale_MQX_KSDK_1.0.0-KL43Z.bin Linux installer. Freescale MQX™ RTOS software   components fully pre-integrated with the Kinetis SDK. Includes the MQX   kernel, USB host and device stacks, MFS file system, and example   applications. Does not require prior installation of Kinetis SDK. 3 MQXKSDKKL43Z.pdf Freescale MQX™ RTOS for Kinetis   SDK FRDM-KL43Z Freescale Freedom Platform Release Notes ·         Target HW boards: o   Freescale Freedom FRDM-KL43Z platform with a MKL43Z256VLH4 processor ·         Key features:  o   PSP support for the MKL43Z256VLH4 Microcontroller o   BSP for the Freescale Freedom FRDM-KL43Z platform with a MKL43Z256VLH4 processor o   MQX STDLIB o   nShell o   KSDK Support for the MKL43Z256VLH4 Microcontroller o   MFS file system ·         Known issues For known issues and limitations please consult the release
查看全文
Store web pages externally step by step Web pages can be stored on any media accessible via MFS, such as USB memory stick, SD card. It is also possible to use FFS and store web pages on NAND flash. The following example is a step by step guide on how MQX can use nandflash on TWR-K70F120M, we start with the httpsrv demo. 1. Add FTP server  and nandflash flush support This demo starts with default HTTPSRV example, Shell console is enabled in the default httpdsrv.c. Ping, ipconfig and help commands are enabled by default. We add ftpsrv application to support FTP protocol , and nandflash support. 2. Allow RTCS for more sockets We will use two TCP servers. There is one socket need for HTTPSRV listening socket, second listening socket for FTP server. One socket for each connected client. 3 .Add MFS library to the HTTPSRV build project By default, MFS library is not enabled in the HTTPSRV project. It uses only TFS for web pages storage. We add path to MFS library into HTTPSRV build project   4. Add FFS support to the HTTPSRV build project Ffs library is not enabled by default. We need to add path into HTTPSRV build library. Install FFS driver and open it. 5. Resolve build errors When we try to build now the HTTPSRV example, we have compile errors. This is because by default the HTTPSRV example does not include MFS and FFS library head files. We need to add a path for MFS and FFS 6. Configure HTTPSRV root directory Web pages of this demo are to be stored in nandflash within web_pages folder. We need to set rootdir and index Before we can view the web page in browser, we need to copy web pages to nand flash. This is the purpose of FTP server, as one example how to copy files. If you wish to be sure the web pages survive power cycle, make sure you flush the FFS file system after “web_pages” are copied. 7. Build, Download, Execute As hardware we use TWR-K70F120M and TWR-SER. After you download the executable and run, start FTP server by issuing command “ftpsrv  start” on serial console; start FTP client; copy over files from PC host to TWR nandflash. Keep the folder structure of the copied files; now open your web browser (support for HTML5 is required); open Url http://192.168.1.202
查看全文
This is a friendly guide to install MQX.
查看全文
Hello I want to share this document that describes steps to configure and use the MQXLite Performance Tool to analyze and debug the applications of the Freescale MQXLite operating system. I hope this helps!! Regards Soledad
查看全文
MQX RTCS Memory Configuration Parameters Introduction         RTCS uses some global variables when an application creates it. All the variables have default values. If you want to change the values, the application must do so before it creates RTCS. There are various configuration parameters that allow to fine tune RTCS memory usage. Next I will introduce the parameters, and I hope it will help beginners in configuration the RTCS correctly 1    _RTCSPCB / _RTCS_msgpool / _RTCS_socket_part RTCSPCB represents the pool of Packet Control Blocks - the number of packets you want RTCS to handle at any given time. RTCSPCB has influence on losing packets. RTCS_msgpool represents the pool of RTCS messages, used to encapsulate application requests to RTCS – the number of simultaneous application requests to RTCS. RTCS_Sockets represents the pool of sockets – the number of sockets in existence at any point in time. “_init” is pre-allocated count, allocation happens when RTCS starts. During runtime, when RTCS needs more of these resources, it allocates more by "_grow" chunks until the "_max" is consumed, which is the effective limit for RTCS resources. These parameters must be called before _RTCS_start By default these parameters are defined as RTCSCFG_PCBS_INIT, RTCSCFG_PCBS_GROW, RTCS_PCBS_MAX, RTCSCFG_MSGPOOL_INIT, RTCSCFG_MSGPOOL_GROW, RTCSCFG_PCBS_MAX, RTCSCFG_SOCKET_PART_INIT, RTCSCFG_SOCKET_PART_GROW,  RTCSCFG_SOCKET_PART_MAX. In application we can override these defaults by _init, _grow, _max. We also can override these in user_config.h. How to configure these parameters?   We don’t have a formal method how to configure these for a specific application. We can start with the defaults and then spent some time increasing these parameters, then we can use RTCS TAD window to see, what RTCS resources are out. Then increase the one a bit. Example:  the configuration in web_hvac demo _RTCSPCB_init = 4; _RTCSPCB_grow = 2; _RTCSPCB_max = 20; _RTCS_msgpool_init = 4; _RTCS_msgpool_grow = 2; _RTCS_msgpool_max  = 20; _RTCS_socket_part_init = 4; _RTCS_socket_part_grow = 2; _RTCS_socket_part_max  = 20; RTCS_Create(); 2  Tx Window Size and Rx Window Size Each socket requires to allocation Tx and Rx window size for a listening socket and then for each connected client.  The default tx window size and rx window size are 4380 bytes. With TAD, we can see that every new TCP socket connection needs extra 500+4392x2+148=9432B   as follows: MQX -> Lightweight Memory Block Summary Size (Decimal) Owner    Type 500      0x10001 TCP Control Block;RTCS/TCP 4392 0x10001  TCP Tx Window;RTCS/TCP 4392 0x10001  TCP Rx Window;RTCS/TCP 148 0x10001  TCP Send Clock;RTCS/TCP (TCP/IP Task id is 0x10001) If we call setsockopt() to reduce these two buffers, for example,            uint_32 value; … value = 1024; setsockopt(sock, SOL_TCP,OPT_TBSIZE,&value,sizeof(value)); setsockopt(sock, SOL_TCP,OPT_RBSIZE,&value,sizeof(value)); The memory usage to open a new TCP socket will drop as follows: MQX -> Lightweight Memory Block Summary Size (Decimal) Owner    Type 500  -> 500   0x10001  TCP Control Block;RTCS/TCP 4392 -> 1108   0x10001 TCP Tx Window;RTCS/TCP 4392 -> 1108   0x10001  TCP Rx Window;RTCS/TCP 148  -> 84   0x10001  TCP Send Clock;RTCS/TCP So we can see that, every new socket connection needs extra 500+1108*2+84=2800
查看全文
Hi All, The new Freescale MQX™ 4.1.1 GA release is now available on www.freescale.com/mqxrtos ·         Files available           # Name Description 1 FSL_MQX_RELEASE_NOTES_4_1_1 Freescale   MQX™ RTOS 4.1.1 Release Notes 2 Freescale   MQX RTOS 4.1.1 for Linux This   release has the same basic code as the 4.1.1 version, with just the changes   needed to build and debug on Linux systems. 3 Freescale   MQX RTOS 4.1.1 MQX™    Source code. Includes an RTOS, File System, TCP/IP and USB host/device   software stacks. ·         What is New? ·         New Board Support Package o   FRDM-K64F o   TWR-K64F120M ·         New Features and Updates o   MQX RTOS 4.1.1 enables development on Linux machines o   MQX RTOS 4.1.1 supports the new Freescale IDE, Kinetis Design Studio o   Example ISR and related documentation is updated to give guidance on setting up a Kernel ISR (a.k.a Gorilla ISR) - extremely high priority ISR o   Power PC (PX) family support has been dropped o   Readme files are added to examples without a description o   Register definition header files for Kinetis MCUs are added for convenience when porting to an MCU sub-family device o   Both interrupt driven I2C master and slave mode drivers are changed to support synchronous blocking mode and share the same API with the polling driver variant.  Improves performance by eliminating the need to poll for data availability. ·         Known issues o   For known issues and limitations please consult the release notes
查看全文
Freescale MQX incluye un BSP que soporta funciones y periféricos comúnmente usados. Sin embargo en aplicaciones muy específicas puede ser necesario el desarrollo o modificación de uno o varios “Drivers”. El siguiente documento explica cómo crear y agregar un nuevo driver al BSP en MQX. El documento está escrito en español. Espero que les sea útil. Saludos Sol
查看全文
Introduction Official support for MQX in KDS is slated for August of this year (2014), but what if you want to start building up your libraries now? Through Mingw and the files included in MQX 4.1, we can compile libraries and programs using KDS’ gcc_arm compiler. This is essentially a modification of the process used to compile MQX on a generic gcc_arm compiler. Original documentation can be found in: <MQX_ROOT_DIR> \doc\tools\gnu\MQX_GNU_Getting_Started.pdf I will try to explain a bit more of the setup process and the file changes that must be made to correctly compile, along with debugging your executable in processor expert. This guide is written for Windows and a version of the guide including a few screenshots of important screens is attached. Setup You will need: Mingw installed, along with mingsys-SED. This can be found at http://sourceforge.net/projects/mingw/ Make sure ‘c:\MinGW\bin’ has been added to system ‘PATH’ variable SED is part of a cmd improvement suite called mingsys. You can install the whole suite, but we only need SED KDS installed A suitable text editor that allows find and replace of text in all files of a selected directory. I recommend Notepad++ and it is what I will use in the tutorial. MQX file changes The original makefiles and batch scripts were created for gcc_arm v4.7.4, but KDS 1.0.1 is using 4.8.0. This means some directory paths have changed and these changes must be updated within MQX’s files. First, let us define the toolchain for the builder to use, in <MQX_ROOT_DIR> \build\common\make\global.mak, modify the following definition: ifeq ($(TOOL),gcc_arm)      TOOLCHAIN_ROOTDIR = <KDS_INSTALLION_DIR>\toolchain Endif Next we need to update the directory listings for gcc_arm components within its root directory. This comes down to replacing all instances of “/4.7.4/” with “/4.8.0/” in all ‘gcc_arm.mak’ files (you could choose to only edit the .mak files of boards you intend to use,  but it’s just as easy to replace all instances). In notepad++, this is simple process of running a “Find in Files”. The files themselves will be located in directories associated with building mqx for each platform: <MQX_ROOT_DIR> \mqx\build\make\<SPECIFIC_PLATFORM>\tools\gcc_arm.mak Along with some entries within application builds: <MQX_ROOT_DIR> \mqx\examples\<project>\build\make\<project>_<platform>\tools\gcc_arm.mak Lastly, specifically for demo application builds, there is one more directory change and one exclusion to make: remove ‘armv7e-m/’ from directory paths and comment out ‘libnosys.a’ (I must clarify I don’t understand the importance of libnosys and couldn’t find a suitable replacement with KDS’ gcc_arm toolchain. I have build hello2 successfully without it, but maybe other projects will require it) Again, this is a simple ‘Find in Files’, replacing “armv7e-m/” with no characters, then replacing the line: RT_LIBRARIES += $(TOOLCHAIN_ROOTDIR)/arm-none-eabi/lib/armv7e-m/softfp/libnosys.a With #RT_LIBRARIES += $(TOOLCHAIN_ROOTDIR)/arm-none-eabi/lib/armv7e-m/softfp/libnosys.a to comment it out. Building Libraries The build process is now incredible easy, as we can use the batch scripts provided in MQX to build our libraries. Either use “<MQX_ROOT_DIR> \build\<BOARD>\make\ build_gcc_arm.bat” to create the full set of libraries for the chosen board (bsp, psp, usb, shell, mfs,rtcs), or use any “build_gcc_arm.bat” found in the component and board area of your choice. These will automatically build the libraries and move the created libraries and code to ““<MQX_ROOT_DIR> \lib\<BOARD>.gcc_arm\” Note: when building full libraries the system will sometimes throw up errors when calling ‘mkdir’, saying that the folder structure already exists.  I have found if you re-run the script again it will not complain the second time and behaves fine. Building Examples So far only tested ‘hello2’on twrk60n512, but principles should apply to all boards and projects Again, we use the batch scripts provided in MQX, found in locations such as: <MQX_ROOT_DIR>\mqx\examples\<PROJECT>\build\make\<BOARD>\build_gcc_arm.bat Running these batch scripts will create another folder within the directory, called “gcc_arm”, in which you can find “initflash_debug” and “initflash_release”.  Inside each of these folders is your compiled application. Debugging your examples Now let’s actually do something in KDS: debugging the examples and showing that they work. For this you need to have a workspace (otherwise KDS won’t run), but you can close any open projects if you wish.  Then Click on the debug menu and select “Debug Configurations...” Double click on your chosen debug interface and under the option for “C/C++ Application”, choose browse and select the ‘.elf’ file from the ‘initFlashdebug’ folder of your application. I hope this helps some people who need to get MQX running through KDS before the official support becomes available. For information on when MQX will be supported on KDS, see https://community.freescale.com/docs/DOC-95477
查看全文
MQX 4.1.0 provides a USB Host CDC demo in the folder of "C:\Freescale\Freescale_MQX_4_1\usb\host\examples\cdc\cdc_serial", but to get it work, several steps need to be done: 1. Change CDC_EXAMPLE_USE_HW_FLOW in cdc_serial.h to 1. #define CDC_EXAMPLE_USE_HW_FLOW 1 2. In config\twrk70f120m\user_config.h, interrupt mode for UART should be set.//It depends on the platform, here given TWR-K70F120M is used. #define BSPCFG_ENABLE_TTYC 0 #define BSPCFG_ENABLE_ITTYC 1 In mqx\source\bsp\twrk70f120m\twrk70f120m.h, specify 'ittyc' instead of 'ttyc' #ifndef BSP_DEFAULT_IO_CHANNEL #if BSPCFG_ENABLE_ITTYC #define BSP_DEFAULT_IO_CHANNEL "ittyc:" /* OSJTAG-COM polled mode */ #define BSP_DEFAULT_IO_CHANNEL_DEFINED #else #define BSP_DEFAULT_IO_CHANNEL NULL #endif #else 3. In usb\host\source\classes\cdc\usb_host_cdc.c, pass fd_ptr instead of data_instance as the argument. a. Around line 977 //usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_in_data_callback, (void *) data_instance); usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_in_data_callback, (void *) fd_ptr); b. Around line 1116 //usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_in_data_callback, (void *) data_instance); usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_in_data_callback, (void *) fd_ptr); c. Around line 1226 //usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_out_data_callback, (void *) data_instance); usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_out_data_callback, (void *) fd_ptr); With above modification , the Host CDC demo can work with a Device CDC demo, such as the one in "C:\Freescale\Freescale_MQX_4_1\usb\device\examples\cdc\virtual_com", which is an echo demo, it would send back anything charactor that it receives. But to see the echo more clearly, I made it echo back the charactor that greater than what is received, for example, if you type A, and will see B from the HyperTerminal. To do that , you have to change Virtual_Com_App(void) in the virtual_com.c as below: void Virtual_Com_App(void) {     /* User Code */     if(g_recv_size)     {         _mqx_int i;                 /* Copy Buffer to Send Buff */         for (i = 0; i < g_recv_size; i++)         {             printf("Copied: %c\n", g_curr_recv_buf[i]);             g_curr_send_buf[g_send_size++] = g_curr_recv_buf[i]+1;         }         g_recv_size = 0;     }         if(g_send_size)     {         uint8_t error;         uint8_t size = g_send_size;         g_send_size = 0;         error = USB_Class_CDC_Send_Data(g_app_handle, DIC_BULK_IN_ENDPOINT,             g_curr_send_buf, size);         if (!error && !(size % DIC_BULK_IN_ENDP_PACKET_SIZE)) {             /* If the last packet is the size of endpoint, then send also zero-ended packet,             ** meaning that we want to inform the host that we do not have any additional             ** data, so it can flush the output.             */             error = USB_Class_CDC_Send_Data(g_app_handle, DIC_BULK_IN_ENDPOINT, NULL, 0);         }         if(error != USB_OK)         {             /* Failure to send Data Handling code here */         }     }     return; } After you download code into, for example, TWR-K70F120(Host) and TWR-K60D100M(Device), and assemble them with TWR-SER and TWR-ELEV, you may connect them via USB port as below: Please also pay attention to J10(USB VBUS Select) and J16(USB Mode Select) according to the function of each tower system. With HyperTerminal connected with TWR-K70F120M system, you may type in any charactor ended with ENTER, and you will see the charactor echoed back as the attached video. This issue would be fixed in the next release, and sorry for the inconvenience that has caused.
查看全文
The attached document explains how to create a C++ project using CW10.6 with GCC compiler, MQX 4.1. Regards, Carlos
查看全文
The attached document shows how to get the MQX4.1 Virtual Com Port Example. This document is located in the following path: C:\Freescale\Freescale_MQX_4_1\usb\device\examples\cdc\virtual_com Regards, Carlos
查看全文
The new Freescale MQX™ 4.1.0.1 patch release is now available on the www.freescale.com. ·         Files available          # Name Description 1 FSL_MQX_4_1_0_1_RELEASE_NOTE MQX™ RTOS 4.1.0.1 Patch Release Notes 2 Freescale   MQX RTOS 4.1.0.1 Patch This patch release is based on the MQX™ RTOS 4.1.0 release   and provides the solutions to software issues identified in the released   version. ·         Patch Description o   This patch provides the software workarounds for these issues identified in MQX 4.1.0 release: §  IPv6 ping issues ·         Crashes during a ping from an unknown host (IPv6 only). ·         An unhandled interrupt is generated when using the IPv6 ping. §  TCP/UDP issues ·         IPv4 sends an MSS and window size with a SYN. A SYN without an MSS or with a window size zero is dropped by some firewalls. ·         IPv6 UDP close issue. IPv6 only reuses the same IP and port. ·         Fixed the incorrect RTCS_selectset() unblocking. §  APP protocol issues ·         TELNET and Eth_to_serial peformance improvement. ·         HTTPSRV accesses data incorrectly in a session buffer while searching for SSI. ·         FTPSRV session close is missing a shutdown of a data socket. §  BSP issues ·         The TWR-K70F120M BSP is unstable when the DDR2 SDRAM is in high use due to incorrect DDR settings.
查看全文
MQX RTOS developers can now build and debug MQX RTOS on Linux computers right out-of-the-box without extensive setup steps.  Linux support is provided in a separate version of MQX 4.1.0, repackaged for use on Linux systems.  Kinetis & Vybrid BSPs from MQX 4.1.0 are supported.  The new package is in beta stage.  It includes the same basic code as the previous 4.1.0 version, with just the changes needed to build and debug on Linux systems. Download Freescale MQX RTOS 4.1.0 for Linux Beta Depending on the popularity of this release, Freescale may extend Linux support to future MQX RTOS mainline releases.  Stay tuned. Give us your feedback!  Post to the MQX community.  Let us know what you think. Development tools Supported: DS-5 Vybrid Controller Edition 5.16.0  (Vybrid) GNU Tools for ARM Embedded Processors version 4.7-2013-q3  (Kinetis & Vybrid) Here are some brief instructions I put together when using with Ubuntu 12.04: - Download and install gcc for arm (comes with gdb for debugging)   See other post:  gcc compiling + gdb debugging on Kinetis on a Linux host - Kinetis L Examples available - Download and extract the .tar.gz file to a location of your choice    mac@mac-VirtualBox:/$  tar -zxvf Freescale_MQX_4_1_LINUX_beta.tar.gz - Edit global.mk to tell it where your gcc toolchain is located.    mac@mac-VirtualBox:/$ cd <directory where you extracted mqx>/Freescale_MQX_4_1_LINUX_beta/build/common/make/    mac@mac-VirtualBox:/$ vi global.mak    un-comment the section on gcc_arm and set the TOOLCHAIN_ROOTDIR.  For my toolchain gcc is installed to the path /usr/    ifreq ($(TOOL),gcc_arm)        TOOLCHAIN_ROOTDIR  =  /usr/   endif - See  MQX GNU Getting Started Guide for instructions on how to build and debug.     This document is located at /Freescale_MQX_4_1_LINUX_beta/doc/tools/gnu/ Good luck with your next project.  Happy developing!
查看全文
Essentials of MQX RTOS Application Development Free Online Training Series with Videos, Tutorials, and Example Software! 10-Part Series - even more coming later [Scroll down to see all Sessions] Session 1: MQX Architecture and Initialization (20 min) Creating tasks Setting priorities Scheduling Synchronization concepts Introduction to drivers Session 2: Designing for a Multi-Tasking Environment (15 min) Writing applications in a Multi-Tasking Environment Super Loop Programming Limitations, Task Coding Structure Task States What is a blocking call? Task Context Switching Session 3: Task Management and the Scheduler (21 min) How does the MQX scheduler work? Scheduling Policies Priority-based, Time-slice (Round Robin) Selecting Priority Levels for Tasks What is the Task Template List? Using Tasks in your Application Session 4: Synchronization and Message Passing (17 min) What is Synchronization?  What is it used for? Data Flow, Control Flow, Mutual Exclusion Synchronization Options Events, Semaphores, Mutexes, Message Passing Message Passing Types of Message Pools, Message Pool Creation, Sending and Receiving, Light-weight Message Passing Session 5: Introduction to Drivers (28 min) Driver Architecture and options Block vs. Byte modes, POSIX drivers, Low level drivers, Polled vs. Interrupt modes Driver Initialization I/O Subsystem (POSIX) Serial Driver Details Light-weight GPIO Driver Details Session 6: Interrupts (15 min) Interrupts and the scheduler Techniques for writing an ISR Hardware Vector Table Nested Interrupts MQX Interrupt ISR Table Installing ISRs Default Interrupt handler Session 7: Light Weight Events (15 min) Overview of events Working with light-weight & full-featured events Ways to wait on an event Session 8: Light Weight Timers (17 min) One shot vs periodic timers Use cases for timers Working with correlated timers Writing timer Interrupt Service Routines (ISRs) Light weight timers & timer queues Timers and the timer task Session 9: Light Weight ADC Driver (18 min) Light-weight ADC driver (LWADC) Details Attributes of ADCs Configuring and reading ADCs Scaling the ADC output Session 10: Logging (23 min) What is logging?  Why use logs? Working with light-weight logs Working with kernel logging Logging MQX function and ISR entries and exits, task and stack usage Working with full-featured logs
查看全文
May 7, 2014   MQX plugins were rebuilt to support latest DS5.18.   Zip attached to this email contains following plugins:   - com.freescale.projectofprojects   - com.freescale.buildtoolbar   - com.freescale.mqx.configuration.editor   The plugins installation procedure is described in the MQX DS5 getting started manual (chapter 2). Plugins are backward compatible and should work also in older DS5 versions.   https://community.freescale.com/thread/323233   Regards, David Seymour
查看全文
Hi, I want to share a document, the purpose of this document is to indicate step by step how to get the memory footprint of a MQX project. The Freescale MQX RTOS includes the tool Codesize.exe, this document is a guide for people who want to use this tool in order to know the memory RAM/ROM utilization of a MQX project. Regards Soledad
查看全文
The new Freescale MQX™ RTOS 4.1.0 FRDM-K64F release is now available on the www.freescale.com ·         Files available # Name Description 1 FSL_MQX_FRDM-K64F_RELEASE_NOTES Freescale   MQX™ RTOS 4.1.0 FRDM-K64F Release Notes 2 Freescale   MQX RTOS 4.1.0 for the FRDM-K64F Includes   an RTOS, File System, TCP/IP and USB host/device software stacks. Does not   require MQX™ 4.1 installation. ·         Target HW board o   FRDM-K64F ·         New features o   PSP support for the Kinetis K64F o   BSP for the FRDM-K64F development board o   Standard set of I/O drivers supporting the K64F peripherals including: §  LWGPI/O driver §  Serial interrupt and polled driver §  SPI driver §  I2C interrupt and polled driver §  LWADC §  Flash Driver §  RTC Driver §  PIT Timer §  LPT Timer §  WDOG §  Low-power Mode §  SAI §  DMA §  SD Card §  Ethernet driver o   USB Host and Device drivers and stacks o   Example and demo applications demonstrating MQX, USB, RTCS, and MFS usage ·         Known issues o   For known issues and limitations please consult the release notes.
查看全文