mpc5643l_etimer Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc5643l_etimer Interrupt

1,681 Views
lanhuahua
Contributor I

Hi,

I used  MPC5643L LSM mode .This test has 2  fuction :

fuction 1 :eTimer1 channel3_frequency_measurement with Interrupt

fuction 2 :eTimer0 channel0  to generate 20ms interrupt _output PWM signal .

When  JTAGE_test  fuction 1 and  fuction 2, only  fuction 2  work  properly (see adjunck).

What is the problem?

      thanks

Original Attachment has been moved to: mpc5643l_test.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,420 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

There is a working example on our forum:

Example MPC5744P eTimer frequency measurement

It is for different processor but eTimer module is the same.

Just follow the example.

Peter

0 Kudos
Reply