linking single elf file for multiple bootloader and applicationn

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

linking single elf file for multiple bootloader and applicationn

902 次查看
Tarek72
Contributor I

I'm currently trying to get a bootmanager/ bootloader/application to be linked as a single .elf file for the MPC5748G.

There are some issues that I'm a little confused about, and I would be very grateful if you could provide any guidance with regard to them.

The plan is to always boot the bootmanager and then jump to the application or the application according to the value of some flag. How to combine all 3 software entities into one instead of flashing each one on its own and I manage to do that would I be able to access the code of bootloader or application after jumping.

I have already defined different start and end addresses of each entity in the linker file and developed the jumping mechanism

0 项奖励
回复
3 回复数

858 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Tarek72 

I can see two basic options:

1. Generate binary files for additional projects (bootmanager, bootloader) using this method:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Generate-S-Record-Intel-HEX-Bina...

And then import them to your application like this:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Link-a-binary-file-s-into-the-ap...

When you build the application, it will contain all the images.

2. I don't know what kind of tools you use, but if it is S32 Design Studio and Pemicro, you can simply specify here which additional object files should be loaded with the project:

lukaszadrapa_0-1739270151657.png

 

Regards,

Lukas

0 项奖励
回复

843 次查看
Tarek72
Contributor I

okay , which one of these options will allow me to debug the other projects?

0 项奖励
回复

831 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 项奖励
回复