eTPU2 error CW getting function sets

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eTPU2 error CW getting function sets

2,772件の閲覧回数
daniel_fernande
Contributor III

Hello, 

It seems not possible to create a etpu2 CW function set all motor control function on it (PMSM + FOC + AS + Resolver+ QD)

I get this error : 

"

eTPU Function Selector

There was an ERROR during the creation of your eTPU function set.
If the issue persists, please submit a Service Request.

Sorry for the inconvenience."
I checked with different browsers (Chrome, firefox, IE) and a collegue has the same issue.
Could you please have a look?
Thanks, 
Daniel
0 件の賞賛
返信
5 返答(返信)

2,602件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Now it is corrected and it seems it is working fine.

0 件の賞賛
返信

2,602件の閲覧回数
daniel_fernande
Contributor III

Thanks it is working now.

A comment about this, the other motor control eTPU function (for exemple PWMM) seem also different between eTPU and eTPU2 (different size)

I have actually an issue where the PWMM eTPU1 function works and the eTPU2 version doesnt work (see https://community.nxp.com/thread/498000)

Thanks again, 

Daniel

0 件の賞賛
返信

2,602件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, yesterday functions from motor control set has been updated. Please check it again and let me know if the issue disappear.

0 件の賞賛
返信

2,602件の閲覧回数
daniel_fernande
Contributor III

Just checked : issue is still there...

0 件の賞賛
返信

2,602件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is known to me. I have already discussed with eTPU expert.

The problem is (as it is currently placed in the CodeWarrior eTPU Function Selector) QD function is only written for eTPU2 and the rest of motor control library is only written for eTPU and this way it can currently be downloaded as two function sets. Otherwise the compiler reports mentioned error.

It has been reported and it should be corrected very early.

0 件の賞賛
返信