Syntax errors in codewarrior for eTPU 10.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Syntax errors in codewarrior for eTPU 10.3

跳至解决方案
2,064 次查看
InhyeokHwang
Contributor III

Hi,

I wonder why these syntax errors are shown when I build my project.

This is EngineControlSet from AN4907SW.

In the problems window, only warnings are shown but I can find these syntax errors on the code side.

KakaoTalk_20230428_132852274.png

 

KakaoTalk_20230428_132849433.png

 

Do I need to use a specific compiler from ByteCraft?
What I've done is just install cw10.3 for etpu, import project, and build.

Thanks 

标记 (1)
0 项奖励
回复
1 解答
2,050 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

As I know there are 3 different syntaxes for eTPU code development:

- Bytecraft i.e. original functions based on eTPU Function Selector: https://www.nxp.com/webapp/etpu/
- CodeWarrior for eTPU i.r. function based on CW eTPU Function Selector: https://www.nxp.com/webapp/etpu_cw/
- AshWare based on ETEC compiler

If you have source files based on CodeWarrior for eTPU you should be able to used it in CW10.3

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,051 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

As I know there are 3 different syntaxes for eTPU code development:

- Bytecraft i.e. original functions based on eTPU Function Selector: https://www.nxp.com/webapp/etpu/
- CodeWarrior for eTPU i.r. function based on CW eTPU Function Selector: https://www.nxp.com/webapp/etpu_cw/
- AshWare based on ETEC compiler

If you have source files based on CodeWarrior for eTPU you should be able to used it in CW10.3

0 项奖励
回复