Syntax errors in codewarrior for eTPU 10.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Syntax errors in codewarrior for eTPU 10.3

ソリューションへジャンプ
2,045件の閲覧回数
InhyeokHwang
Contributor III

Hi,

I wonder why these syntax errors are shown when I build my project.

This is EngineControlSet from AN4907SW.

In the problems window, only warnings are shown but I can find these syntax errors on the code side.

KakaoTalk_20230428_132852274.pngKakaoTalk_20230428_132852274.png

KakaoTalk_20230428_132849433.pngKakaoTalk_20230428_132849433.png

Do I need to use a specific compiler from ByteCraft?
What I've done is just install cw10.3 for etpu, import project, and build.

Thanks 

タグ(1)
0 件の賞賛
返信
1 解決策
2,031件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

As I know there are 3 different syntaxes for eTPU code development:

- Bytecraft i.e. original functions based on eTPU Function Selector: https://www.nxp.com/webapp/etpu/
- CodeWarrior for eTPU i.r. function based on CW eTPU Function Selector: https://www.nxp.com/webapp/etpu_cw/
- AshWare based on ETEC compiler

If you have source files based on CodeWarrior for eTPU you should be able to used it in CW10.3

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,032件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

As I know there are 3 different syntaxes for eTPU code development:

- Bytecraft i.e. original functions based on eTPU Function Selector: https://www.nxp.com/webapp/etpu/
- CodeWarrior for eTPU i.r. function based on CW eTPU Function Selector: https://www.nxp.com/webapp/etpu_cw/
- AshWare based on ETEC compiler

If you have source files based on CodeWarrior for eTPU you should be able to used it in CW10.3

0 件の賞賛
返信