Startup Problem MPC5746C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Startup Problem MPC5746C

1,961 Views
eyupozer
Contributor III

Hi,

I have a problem regarding the program startup sequence for MPC5746C MCU with the S32 design studio.

Program is not running properly when I run step by step, the program is crashing after that "startup_MPC5746C.s" line 159 "mtmsr r6" command.

What is the problem? Is there a hardware or software problem?

could you please explain this problem if it can be solved.

Thanks.

pastedImage_2.png

0 Kudos
Reply
3 Replies

1,828 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I guess you have pending Machine check and once you enable it your device will jump into IVOR1

pastedImage_2.png

pastedImage_1.png

If you share with me compiled code you are using I can check where is the issue as from the screenshot I am not able to tell you the root cause.

regards,

Peter

0 Kudos
Reply

1,828 Views
eyupozer
Contributor III

Hi,

Thanks for your response Peter,

I can share the compiled code but this problem exists for all program for this MCU. Other word Program independent.

can we say the MCU has a hardware error?

0 Kudos
Reply

1,828 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Do you serve IVOR1 in your code?

You can try all our example codes and see that there is no issue with MCU:

https://community.nxp.com/docs/DOC-329623 

Furthermore, did you used our EVB or your custom designed board?

Share some more info regarding your setup, project, etc...

regards,

Peter

0 Kudos
Reply