Serial bootloader example for MPC5634M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial bootloader example for MPC5634M

19,059 Views
raphc63
Contributor II

Hi everyone,

I recently bought a MPC563xM StarterTRAK Development Kit. MPC5634M is not supported by RAppID, that's the reason why I want to code my own bootloader for reading, erasing, and writing data on flasH.
Is there a documentation with simple examples of serial bootloader for MPC56xx or MPC55xx which are similar. It will be very helpful for me, this is the first bootloader I have to code.

Labels (1)
27 Replies

3,840 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hello Aleksandar,

I do not have such project for MPC5748G.

The principle is still the same but rework is necessary, of course. What has changed is the memory map, the flash sits at another addresses. There's LINFlex module instead of eSCI, so the functions for serial communication must be changed. (FYI: I will share simple project which includes simple UART communication this or next week). The flash module is different. If it helps, I already shared these two examples for flash programming:

Example MPC5748G Flash RW

Example MPC5748G Flash RW SSD

Lukas

2,381 Views
alexvinchev
Contributor V

Hi Lukas,

I really appreciate your guidance. The two projects for Flash R/W will help of course.

Flash partitioning is bothering me more, this was the reason to ask for example. There are quite much different flash regions and sizes, from where I should pick some part, but which exactly... If you can say few words regarding this, will be very helpful.

Regarding the UART, I've already ported ChibiOS RTOS with CAN & UART drivers (based on AN4830 examples) on MPC5748G, so there is no need to hurry (for me), I think I'll handle UART communication by myself.

Regards,

Aleksandar

0 Kudos
Reply

2,381 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

In case of MPC5634M, there were following options where to put boot header (RCHW):

pastedImage_0.png

In the example project, I allocated first 64KB for bootloader and the rest of flash for application. That means the RCHW for bootloader is at address 0x0000_0000, for application at 0x0001_0000.

In case of MPC5748G, we can put boot header at:

pastedImage_1.png

So, boot header for bootloader can be placed at 0x00F8_C000. If 80Kb is enough for your bootloader, you can place boot header for application at 0x00FE_0000 (or any other, depends on you). Then you have to change the linker files accordingly.

Next point is the Read-While-Write (RWW) partitioning on flash. As you know, we can't access the flash partition which is currently being programmed or erased. The code must run from another partition or from RAM. Here is the partitioning of MPC5748G flash:

pastedImage_2.png

The disadvantage is that the partitions do not create continuous space (for example, partition 0 is split to four non-continuous sections), so we have to be careful where to run the code from to avoid RWW issues.

If you need anything else, just let me know...

Lukas

2,381 Views
alexvinchev
Contributor V

Thank you very much Lukas!

Very helpful advice (again)!

I think I'll sacrifice 0x74000 bytes till 0x01000000 for bootloader and the rest will be for application. This way I'll have no worries regarding RWW issues, because my application will always reside in partitions 6-9 and never touch partitions 0-3.

Does this sounds like a good idea to you?

In case I want to debug application without bootloader, I will use dedicated link file, which will place the boot record in the search area of BAF.

Aleksandar

0 Kudos
Reply

2,381 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, that's a good idea. If you don't have memory constraints, this is the best option.

Lukas

0 Kudos
Reply

2,381 Views
raphc63
Contributor II

Thanks Lukas. I try to understand this project but I have a question.

There are outstring generate by the main program like this example :

OutStr("\f\r\n**********************************************\r\n");

OutStr("\r\nMPC55xx/56xx Bootloader v1.0\r\n");

OutStr("\r\n**********************************************\r\n");

 

Where can I get this outstr on my PC ? And how can I answer to swich menu choice ?  When I execute the program I have no control window.

Thanks

0 Kudos
Reply

2,381 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you need some kind of terminal emulation program like Microsoft HyperTerminal or similar. For example, I use this one (it is freeware):

https://sites.google.com/site/terminalbpp/Terminal20141030.zip

Then you need serial COM port on your PC or USB to serial bridge.

"And how can I answer to swich menu choice ?" - Just send a character from terminal to microcontroller...

Regards,

Lukas

0 Kudos
Reply