The example does exactly the same operation like this example:
https://community.freescale.com/docs/DOC-105380
...but SSD flash driver is used now.
********************************************************************************
* Detailed Description:
*
* Unlock, erase and program of flash mid block 0x00FB_8000 - 0x00FB_FFFF.
* Used SSD flash drivers:
* http://www.freescale.com/files/product/software/C55_JDP_SSD.exe
* Version of the driver is v1.0.0
* ------------------------------------------------------------------------------
* Test HW: X - PC5748G - MB (rev C)
* MCU: PPC5748GMMN6A
* Maskset: 1N81M
* Fsys: 160 MHz
* Debugger: Lauterbach Trace32
*
* Target: Internal_FLASH
*
********************************************************************************