SDADC Pinouts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDADC Pinouts

Jump to solution
2,133 Views
berat24
Contributor III

Hello everyone,

To use sigma delta adc for my CPU called MCP5777C, I looked at the SDADC pins. According to reference manuel, there are analog pins from AN0 to AN7 for sigma delta ADC. However, I cannot understand which I/O ports have this function. For example, If i saw ANB0, I would understand, it is port B.

Could you help me about that?

0 Kudos
Reply
1 Solution
2,123 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is explicitly defined in the excel sheet embedded in the device's RM

davidtosenovjan_0-1623659408354.png

 

View solution in original post

0 Kudos
Reply
2 Replies
2,120 Views
berat24
Contributor III

Thanks a lot:)) @davidtosenovjan 

0 Kudos
Reply
2,124 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is explicitly defined in the excel sheet embedded in the device's RM

davidtosenovjan_0-1623659408354.png

 

0 Kudos
Reply