SDADC Pinouts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,127件の閲覧回数
berat24
Contributor III

Hello everyone,

To use sigma delta adc for my CPU called MCP5777C, I looked at the SDADC pins. According to reference manuel, there are analog pins from AN0 to AN7 for sigma delta ADC. However, I cannot understand which I/O ports have this function. For example, If i saw ANB0, I would understand, it is port B.

Could you help me about that?

0 件の賞賛
返信
1 解決策
2,117件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is explicitly defined in the excel sheet embedded in the device's RM

davidtosenovjan_0-1623659408354.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,114件の閲覧回数
berat24
Contributor III

Thanks a lot:)) @davidtosenovjan 

0 件の賞賛
返信
2,118件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is explicitly defined in the excel sheet embedded in the device's RM

davidtosenovjan_0-1623659408354.png

 

0 件の賞賛
返信