Running higher CLK frequency than specified

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running higher CLK frequency than specified

Jump to solution
4,354 Views
sagardhavali
Contributor III

Our original design was with the SPC5742PFK1AMLQ8 (180MHz rating) but due to lack of availability, modules were built with SPC5744PFK1AMLQ9 (200MHz)

 

Unfortunately, the software is running at the max frequency of the temporary micro (SPC5744PFK1AMLQ9, 200MHz).  So, today, we have production parts built up with the production intent micro, rated for 180MHz.  

Our question is what are the risks involved with running the micro rated for 180MHz at a higher frequency of 200MHz?

Thanks,
Sagar

Labels (1)
Tags (2)
1 Solution
1,868 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

There could be various issue starting from dumping flash lifetime, more heat, EMC, etc...

We do not guarantee micro correct operation when you violate datasheet specifications.

Peter

View solution in original post

2 Replies
1,869 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

There could be various issue starting from dumping flash lifetime, more heat, EMC, etc...

We do not guarantee micro correct operation when you violate datasheet specifications.

Peter

1,868 Views
sagardhavali
Contributor III

Thanks Peter.

Can you please answer my other thread?

0 Kudos
Reply