Running higher CLK frequency than specified

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Running higher CLK frequency than specified

跳至解决方案
4,347 次查看
sagardhavali
Contributor III

Our original design was with the SPC5742PFK1AMLQ8 (180MHz rating) but due to lack of availability, modules were built with SPC5744PFK1AMLQ9 (200MHz)

 

Unfortunately, the software is running at the max frequency of the temporary micro (SPC5744PFK1AMLQ9, 200MHz).  So, today, we have production parts built up with the production intent micro, rated for 180MHz.  

Our question is what are the risks involved with running the micro rated for 180MHz at a higher frequency of 200MHz?

Thanks,
Sagar

标签 (1)
标记 (2)
1 解答
1,861 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

There could be various issue starting from dumping flash lifetime, more heat, EMC, etc...

We do not guarantee micro correct operation when you violate datasheet specifications.

Peter

在原帖中查看解决方案

2 回复数
1,862 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

There could be various issue starting from dumping flash lifetime, more heat, EMC, etc...

We do not guarantee micro correct operation when you violate datasheet specifications.

Peter

1,861 次查看
sagardhavali
Contributor III

Thanks Peter.

Can you please answer my other thread?

0 项奖励
回复