Register test and Program counter test for MPC5602D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Register test and Program counter test for MPC5602D

2,337 Views
ChristopheLEGUERN
Contributor I

Hello,

Is there any library or guideline available to implement CPU register test and program counter test (60730-1 class B) for MPC5602D ?

(I only need to implement these 2 tests items, not the full standard selftest set)

Thank you and regards

Chris

0 Kudos
Reply
3 Replies

2,328 Views
naveenm
NXP Employee
NXP Employee

 

Hi,

Primarily, SafeAssure community is intended to support Safety related queries. This question appears to be functional/architectural, therefore moving it to product group.

Regards,

NaveenM

0 Kudos
Reply

2,322 Views
ChristopheLEGUERN
Contributor I

Hi, my request is related to safety : this CPU self tests are for safety and the UL60730-1 standard also.

0 Kudos
Reply

2,279 Views
naveenm
NXP Employee
NXP Employee

Hi,

Unfortunately, there are no guidelines available on implementation of core tests.

Regards,

NaveenM

0 Kudos
Reply