Register test and Program counter test for MPC5602D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Register test and Program counter test for MPC5602D

2,350件の閲覧回数
ChristopheLEGUERN
Contributor I

Hello,

Is there any library or guideline available to implement CPU register test and program counter test (60730-1 class B) for MPC5602D ?

(I only need to implement these 2 tests items, not the full standard selftest set)

Thank you and regards

Chris

0 件の賞賛
返信
3 返答(返信)

2,341件の閲覧回数
naveenm
NXP Employee
NXP Employee

 

Hi,

Primarily, SafeAssure community is intended to support Safety related queries. This question appears to be functional/architectural, therefore moving it to product group.

Regards,

NaveenM

0 件の賞賛
返信

2,335件の閲覧回数
ChristopheLEGUERN
Contributor I

Hi, my request is related to safety : this CPU self tests are for safety and the UL60730-1 standard also.

0 件の賞賛
返信

2,292件の閲覧回数
naveenm
NXP Employee
NXP Employee

Hi,

Unfortunately, there are no guidelines available on implementation of core tests.

Regards,

NaveenM

0 件の賞賛
返信