Question on PMC_REE_0 Register - MPC5744P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question on PMC_REE_0 Register - MPC5744P

ソリューションへジャンプ
1,845件の閲覧回数
meedandeys
Contributor III

Hello,

Can anyone please explain me what is difference between two bits of the PMC_REE_0 register ?
VD3RE_C - Voltage Detect 3 Reset Enable Cold (Core LVD: 1.25 V).
VD3RE_H - Voltage Detect 3 Reset Enable Hot (Core LVD: 1.25 V).

Thanks

0 件の賞賛
返信
1 解決策
1,704件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Hot means that voltage detector is located in middle of chip where temperature is higher.

Cold means it is located in the corners of chip.

Peter

元の投稿で解決策を見る

2 返答(返信)
1,705件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Hot means that voltage detector is located in middle of chip where temperature is higher.

Cold means it is located in the corners of chip.

Peter

1,704件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello meedandeys‌,

 

Here on the Model-Based Design community we handle questions regarding our toolbox or other MATLAB/Simulink related questions. I think your question is best suited for the https://community.nxp.com/community/s32/mpc5xxx  community, so my advice is to ask it there (as I can not move it myself).

 

As an alternative you could open a ticket for technical support here (go to 'Go to Ticket').

 

Kind regards,

Razvan.

0 件の賞賛
返信