Question on PMC_REE_0 Register - MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question on PMC_REE_0 Register - MPC5744P

Jump to solution
1,850 Views
meedandeys
Contributor III

Hello,

Can anyone please explain me what is difference between two bits of the PMC_REE_0 register ?
VD3RE_C - Voltage Detect 3 Reset Enable Cold (Core LVD: 1.25 V).
VD3RE_H - Voltage Detect 3 Reset Enable Hot (Core LVD: 1.25 V).

Thanks

0 Kudos
Reply
1 Solution
1,709 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Hot means that voltage detector is located in middle of chip where temperature is higher.

Cold means it is located in the corners of chip.

Peter

View solution in original post

2 Replies
1,710 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Hot means that voltage detector is located in middle of chip where temperature is higher.

Cold means it is located in the corners of chip.

Peter

1,709 Views
constantinrazva
NXP Employee
NXP Employee

Hello meedandeys‌,

 

Here on the Model-Based Design community we handle questions regarding our toolbox or other MATLAB/Simulink related questions. I think your question is best suited for the https://community.nxp.com/community/s32/mpc5xxx  community, so my advice is to ask it there (as I can not move it myself).

 

As an alternative you could open a ticket for technical support here (go to 'Go to Ticket').

 

Kind regards,

Razvan.

0 Kudos
Reply