Question of MPC5777C MPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question of MPC5777C MPU

跳至解决方案
3,216 次查看
Luke_Chun
NXP Employee
NXP Employee

Hello Team

 

Could you check about the question of MPC5777C MPU?

As far as I know, 5777C’s MPU does not have Slave port to Flash like below block.

 

174170_174170.pngpastedImage_1.png

 

 

 

 

 

 

However, as the RM of 5777C, it shows like below table for the explanation of Overlapping region.

174171_174171.pngpastedImage_2.png

 


It makes the confusing, why it shows “Flash”…about RGD0 and 1. It looks like that MPC can be used for Flash by 5777C
Could you let me know the reason of Flash?(Is 5777C’s MPU possible to use Flash?)

 


Thank you.

标签 (1)
1 解答
2,798 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I can confirm flash memory is not protected by MPU.

I agree section "14.7 Application information" is misleading as it is apparently some generic example applicable for other devices where it is mostly possible. I will ask for documentation change. Thanks for highlighting of the issue.

在原帖中查看解决方案

4 回复数
2,799 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I can confirm flash memory is not protected by MPU.

I agree section "14.7 Application information" is misleading as it is apparently some generic example applicable for other devices where it is mostly possible. I will ask for documentation change. Thanks for highlighting of the issue.

2,798 次查看
taeyoungchung
Contributor I

If so, the block diagram of MPC5557C in NXP homepage as below is wrong?

This BD looks like flash memory could be protected by MPU.

MPC5777C.jpg

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/32-bit-power-archite...

0 项奖励
回复
2,798 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is not up-to date.

0 项奖励
回复
2,798 次查看
taeyoungchung
Contributor I

Thanks a lot.

0 项奖励
回复