Question of MPC5777C MPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question of MPC5777C MPU

Jump to solution
2,333 Views
Luke_Chun
NXP Employee
NXP Employee

Hello Team

 

Could you check about the question of MPC5777C MPU?

As far as I know, 5777C’s MPU does not have Slave port to Flash like below block.

 

174170_174170.pngpastedImage_1.png

 

 

 

 

 

 

However, as the RM of 5777C, it shows like below table for the explanation of Overlapping region.

174171_174171.pngpastedImage_2.png

 


It makes the confusing, why it shows “Flash”…about RGD0 and 1. It looks like that MPC can be used for Flash by 5777C
Could you let me know the reason of Flash?(Is 5777C’s MPU possible to use Flash?)

 


Thank you.

Labels (1)
1 Solution
1,915 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I can confirm flash memory is not protected by MPU.

I agree section "14.7 Application information" is misleading as it is apparently some generic example applicable for other devices where it is mostly possible. I will ask for documentation change. Thanks for highlighting of the issue.

View solution in original post

4 Replies
1,916 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I can confirm flash memory is not protected by MPU.

I agree section "14.7 Application information" is misleading as it is apparently some generic example applicable for other devices where it is mostly possible. I will ask for documentation change. Thanks for highlighting of the issue.

1,915 Views
taeyoungchung
Contributor I

If so, the block diagram of MPC5557C in NXP homepage as below is wrong?

This BD looks like flash memory could be protected by MPU.

MPC5777C.jpg

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/32-bit-power-archite...

0 Kudos
Reply
1,915 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is not up-to date.

0 Kudos
Reply
1,915 Views
taeyoungchung
Contributor I

Thanks a lot.

0 Kudos
Reply