Pin eMIOS5/eTPUA5/GPIO184 can't be used as eMIOS-input?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin eMIOS5/eTPUA5/GPIO184 can't be used as eMIOS-input?

ソリューションへジャンプ
2,206件の閲覧回数
martinklonfar
Contributor I

Hi,

On MPC5777C, I need to use eMIOS5 in SAIC mode. However, when I assign the eMIOS-function to the pin (SIU_PCR184 = 0x0503), the input signal almost disappears and eMIOS5 never detects any edge. Checking the pin with multimeter I found out that its resistance against GND drops to some 14-15 Ohm after assigning the eMIOS-function - hence the "disappearance" of the input signal.

Temporary re-wiring to eMIOS23 solved the issue, but that's not a long-term option.

Is it possible to use the eMIOS-input function on this pin?

0 件の賞賛
返信
1 解決策
2,181件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

words from RM's chapter 3.5 External signal descriptions, multiplexing, and attributes...
Details about external signal functions, their static electrical characteristics, and pad configuration settings for this chip appear in the spreadsheet that is embedded within this document:
MPC5777C_System_IO_Definition.xlsx
To access this spreadsheet, view the document's list of attachments.

PetrS_0-1671133491226.png

BR, Petr

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,191件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no, it is not possible to use pin for eMIOS input, it is output only pin

PetrS_0-1671090719449.png

BR, Petr

0 件の賞賛
返信
2,186件の閲覧回数
martinklonfar
Contributor I

Thanks for explaining. Which document is Your screenshot taken from, please? Because I need to identify all eMIOS channels with this feature ...

0 件の賞賛
返信
2,182件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

words from RM's chapter 3.5 External signal descriptions, multiplexing, and attributes...
Details about external signal functions, their static electrical characteristics, and pad configuration settings for this chip appear in the spreadsheet that is embedded within this document:
MPC5777C_System_IO_Definition.xlsx
To access this spreadsheet, view the document's list of attachments.

PetrS_0-1671133491226.png

BR, Petr

 

0 件の賞賛
返信