Pin eMIOS5/eTPUA5/GPIO184 can't be used as eMIOS-input?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin eMIOS5/eTPUA5/GPIO184 can't be used as eMIOS-input?

Jump to solution
2,184 Views
martinklonfar
Contributor I

Hi,

On MPC5777C, I need to use eMIOS5 in SAIC mode. However, when I assign the eMIOS-function to the pin (SIU_PCR184 = 0x0503), the input signal almost disappears and eMIOS5 never detects any edge. Checking the pin with multimeter I found out that its resistance against GND drops to some 14-15 Ohm after assigning the eMIOS-function - hence the "disappearance" of the input signal.

Temporary re-wiring to eMIOS23 solved the issue, but that's not a long-term option.

Is it possible to use the eMIOS-input function on this pin?

0 Kudos
Reply
1 Solution
2,159 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

words from RM's chapter 3.5 External signal descriptions, multiplexing, and attributes...
Details about external signal functions, their static electrical characteristics, and pad configuration settings for this chip appear in the spreadsheet that is embedded within this document:
MPC5777C_System_IO_Definition.xlsx
To access this spreadsheet, view the document's list of attachments.

PetrS_0-1671133491226.png

BR, Petr

 

View solution in original post

0 Kudos
Reply
3 Replies
2,169 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no, it is not possible to use pin for eMIOS input, it is output only pin

PetrS_0-1671090719449.png

BR, Petr

0 Kudos
Reply
2,164 Views
martinklonfar
Contributor I

Thanks for explaining. Which document is Your screenshot taken from, please? Because I need to identify all eMIOS channels with this feature ...

0 Kudos
Reply
2,160 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

words from RM's chapter 3.5 External signal descriptions, multiplexing, and attributes...
Details about external signal functions, their static electrical characteristics, and pad configuration settings for this chip appear in the spreadsheet that is embedded within this document:
MPC5777C_System_IO_Definition.xlsx
To access this spreadsheet, view the document's list of attachments.

PetrS_0-1671133491226.png

BR, Petr

 

0 Kudos
Reply