PIT timer does not run during online debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PIT timer does not run during online debugging

Jump to solution
1,367 Views
wxf
Contributor I

dear all,

 

 

  When I debug online, when the PIT timer is set to non-freeze mode, it can count normally, but if it is set to freeze mode, the timer never counts, even when it is running at full speed.


  What could be the cause of this?

 

tank you!

 XiufengWang

0 Kudos
Reply
1 Solution
1,363 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

It's known issue in S32DS debugger affecting MPC56xx/57xx devices. It was already discussed here, for example:

https://community.nxp.com/t5/MPC5xxx/stuck-in-OSIF-TimeDelay/m-p/1354830

Regards,

Lukas

View solution in original post

0 Kudos
Reply
1 Reply
1,364 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

It's known issue in S32DS debugger affecting MPC56xx/57xx devices. It was already discussed here, for example:

https://community.nxp.com/t5/MPC5xxx/stuck-in-OSIF-TimeDelay/m-p/1354830

Regards,

Lukas

0 Kudos
Reply