PIT timer does not run during online debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PIT timer does not run during online debugging

ソリューションへジャンプ
1,360件の閲覧回数
wxf
Contributor I

dear all,

 

 

  When I debug online, when the PIT timer is set to non-freeze mode, it can count normally, but if it is set to freeze mode, the timer never counts, even when it is running at full speed.


  What could be the cause of this?

 

tank you!

 XiufengWang

0 件の賞賛
返信
1 解決策
1,356件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

It's known issue in S32DS debugger affecting MPC56xx/57xx devices. It was already discussed here, for example:

https://community.nxp.com/t5/MPC5xxx/stuck-in-OSIF-TimeDelay/m-p/1354830

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,357件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

It's known issue in S32DS debugger affecting MPC56xx/57xx devices. It was already discussed here, for example:

https://community.nxp.com/t5/MPC5xxx/stuck-in-OSIF-TimeDelay/m-p/1354830

Regards,

Lukas

0 件の賞賛
返信