PIT Interrupt handling in MPC5777C on Core1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PIT Interrupt handling in MPC5777C on Core1

1,138 次查看
hemantsindkar
Contributor III

Hi,

 

I am facing issue in PIT interrupt handling in MPC5777C on core1.

I am using PIT1 for Core0 which is working fine. When interrupt flag bit set interrupt ISR get fired.

I am using PIT2 for Core1 which is not working. When interrupt occurs interrupt flag bit set but interrupt ISR not get fired.

 

Thanks & Regards

Hemant

标签 (1)
0 项奖励
回复
1 回复

852 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have just posted example code that it blinking one LED by Core0 and PIT0 and second LED by Core1 and PIT2.

Here is the link:

Example MPC5777C-PinToggleStationery GHS614

0 项奖励
回复