MPC5746R, Hardware Design for MPC5746R Emulation Device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5746R, Hardware Design for MPC5746R Emulation Device

1,338件の閲覧回数
hongpingxu-b364
NXP Employee
NXP Employee

Hi.


Customer use MPC5746R (Rainier) Emulation Device (292-MAPBGA package). Something need be clarified as below:
- VDD_HV_IO_BD pin, supply 3.3V or 5V for this PIN?
- VDD_LV_BD supply voltage is 1.2V. where is the power supply the 1.2V, from VDD_LV? from external 1.2V power?
- How to use pin LVDS_TEST_N and LVDS_TEST_P? Connect to 3.3V/5V or Ground, or no connection?


Thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

1,084件の閲覧回数
Shanaka_Yapa
NXP Employee
NXP Employee

- VDD_HV_IO_BD should be 5V, it can be tied with VDD_HV_IO_MAIN, VDD_LV_BD can be supplied externally nominal 1.25V or VDD_LV but the supply need to be capable to provide enough current than the normal MPC5746R spec in DS. Regarding the power sequencing PD(Production Die supplies ex VDD_LV, VDD_HV_IO_MAIN etc) & Buddy supplied need to be powered up same time or Buddy need to be powered first then the PD.

- LVDS_TEST_N and LVDS_TEST_P should be NC ( No connect)

also refer the AN5181, it will give you the NXP Adapter solutions for ED devices.

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5181.pdf?fsrch=1&sr=2&pageNum=1

0 件の賞賛
返信