Non-correctable RAM error MPC5604B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Non-correctable RAM error MPC5604B

2,224件の閲覧回数
aditya_barve
Contributor III

Hello, 

 

I am trying to generate ECC error using EEGR registers. 

When I try to simulate a Non-Correctable error using FRCNCI register, the controller resets. 

Is there any documentation to refer and understand this behavior ?

 

Thank you,

Aditya

0 件の賞賛
返信
3 返答(返信)

2,219件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please refer to AN5200:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/AN5200-Error-Correcting-Codes-Implemented-on-MPC...

Chapter 6:

petervlna_0-1635311286973.pngpetervlna_0-1635311286973.png

Best regards,

Peter

0 件の賞賛
返信

2,217件の閲覧回数
aditya_barve
Contributor III

Thank you for the reference. 

 

Is there any reason why the controller would reset after setting the non-correctable error generation bit ?

 

Thanks,

Aditya

0 件の賞賛
返信

2,213件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

it depends on how you handle exception. If it is unhandled they you will get reset. If the reset is triggered in exception, you will get reset. etc...

refer to : 5.1 Based on IVORx exception

Best regards,

Peter

0 件の賞賛
返信