Non-correctable RAM error MPC5604B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Non-correctable RAM error MPC5604B

2,286 Views
aditya_barve
Contributor III

Hello, 

 

I am trying to generate ECC error using EEGR registers. 

When I try to simulate a Non-Correctable error using FRCNCI register, the controller resets. 

Is there any documentation to refer and understand this behavior ?

 

Thank you,

Aditya

0 Kudos
Reply
3 Replies

2,281 Views
petervlna
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,279 Views
aditya_barve
Contributor III

Thank you for the reference. 

 

Is there any reason why the controller would reset after setting the non-correctable error generation bit ?

 

Thanks,

Aditya

0 Kudos
Reply

2,275 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

it depends on how you handle exception. If it is unhandled they you will get reset. If the reset is triggered in exception, you will get reset. etc...

refer to : 5.1 Based on IVORx exception

Best regards,

Peter

0 Kudos
Reply