MPC5777M DSPI problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777M DSPI problem

1,152件の閲覧回数
underdangerous
Contributor II

Hi,community:

I am a newer in MPC5777M. I want to configure DSPI as DSI mode, but I can not write 2'b01 to DSPI_0.MCR[DCONF]. It can be 00b once I write 01b to it, and I can not write access DSPI_0.ASDR0. Is there any sample code which can help me to understand how to configure DSPI to DSI/CSI mode?  Thx!

0 件の賞賛
返信
1 返信

1,143件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I made a screenshot from older manual, because in current version this table is broken. It is apparent you need to choose DSPI4/5/6 as only these module instances support serialization.

 davidtosenovjan_0-1690446784789.png

I have only tested with MPC5746R device. Example code you find here:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5746R-DSPI-serialization-S32DS-Power-...

 

0 件の賞賛
返信