MPC5748g Flexray clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748g Flexray clock

ソリューションへジャンプ
3,532件の閲覧回数
WM
Contributor II

MPC5748g Flexray clock using PLL how to set

タグ(1)
0 件の賞賛
返信
1 解決策
3,498件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is the configuration

davidtosenovjan_0-1655214789228.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,522件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

You may have two options:
- either 40MHz directly feeded by crystal oscillator
- or 80MHz clock feeded from PLL

I am recommending to use following clock configurator:

https://www.nxp.com/docs/en/application-note/AN5392.pdf

0 件の賞賛
返信
3,505件の閲覧回数
WM
Contributor II

Hello, davidtosenovjan        

    Thank you for your answer.      

     If FR_MCR[CLKSEL] is 1 in MPC5748, check whether other configurations are required in flexray PE clock?  I have configured FS80=80MHz. 

捕获.PNG

0 件の賞賛
返信
3,499件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is the configuration

davidtosenovjan_0-1655214789228.png

 

0 件の賞賛
返信