MPC5748G PinOut

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
8,441件の閲覧回数
michaelm
Contributor I

Hi,

 

I'm new with Freescale Chips in development. Where can I find Pin-Out tables for MPC5748G 176Pin LQFP? There are none at the Freescale download-area...

 

Thank you in advance

Michael

ラベル(1)
1 解決策
7,397件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It is attached in Reference manual.

Peter

元の投稿で解決策を見る

6 返答(返信)
4,623件の閲覧回数
royke
Contributor I

Hello

All links that can be found to this reference manual do not work. Hopefully someone can help with this reference manual

 

With kind regards 

0 件の賞賛
返信
7,397件の閲覧回数
PeterHartlmuell
Contributor I

Hi,

It is understood, that the signal description "is attached in Reference manual".

Nevertheless, I did not find any place to download this Excel file. Is it only available under an NDA?

Greetings, Peter

0 件の賞賛
返信
7,397件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It is an embedded attachment in reference manual pdf format.

pastedImage_1.png

Please find in your pdf browser,viewer or editor the paperclip icon.

Under is are embedded attachment.

Peter

7,398件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It is attached in Reference manual.

Peter

7,397件の閲覧回数
carlvanwormer
Contributor II

The attachment to the rev.5 reference manual document (IO_Signal_Description_and_Input_Multiplexing_Tables.xlsx) has errors in the pin names for both the 176LQFP and the BGA256 packages.  The rev.4 reference manual does not have these errors.  The bad names for 5 of the pins are all "#REF!", which is an Excel error for a bad cell reference.

7,397件の閲覧回数
nathanimig
Contributor I

Hello, so I have been searching intrawebs for rev. 4 and I can't seem to find this anywhere. Is there anyway you could share this, it would be greatly appreciated?

0 件の賞賛
返信