MPC5748G PinOut

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5748G PinOut

跳至解决方案
8,440 次查看
michaelm
Contributor I

Hi,

 

I'm new with Freescale Chips in development. Where can I find Pin-Out tables for MPC5748G 176Pin LQFP? There are none at the Freescale download-area...

 

Thank you in advance

Michael

标签 (1)
1 解答
7,396 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It is attached in Reference manual.

Peter

在原帖中查看解决方案

6 回复数
4,622 次查看
royke
Contributor I

Hello

All links that can be found to this reference manual do not work. Hopefully someone can help with this reference manual

 

With kind regards 

0 项奖励
回复
7,396 次查看
PeterHartlmuell
Contributor I

Hi,

It is understood, that the signal description "is attached in Reference manual".

Nevertheless, I did not find any place to download this Excel file. Is it only available under an NDA?

Greetings, Peter

0 项奖励
回复
7,396 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It is an embedded attachment in reference manual pdf format.

pastedImage_1.png

Please find in your pdf browser,viewer or editor the paperclip icon.

Under is are embedded attachment.

Peter

7,397 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It is attached in Reference manual.

Peter

7,396 次查看
carlvanwormer
Contributor II

The attachment to the rev.5 reference manual document (IO_Signal_Description_and_Input_Multiplexing_Tables.xlsx) has errors in the pin names for both the 176LQFP and the BGA256 packages.  The rev.4 reference manual does not have these errors.  The bad names for 5 of the pins are all "#REF!", which is an Excel error for a bad cell reference.

7,396 次查看
nathanimig
Contributor I

Hello, so I have been searching intrawebs for rev. 4 and I can't seem to find this anywhere. Is there anyway you could share this, it would be greatly appreciated?

0 项奖励
回复