MPC5748G PinOut

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G PinOut

Jump to solution
8,446 Views
michaelm
Contributor I

Hi,

 

I'm new with Freescale Chips in development. Where can I find Pin-Out tables for MPC5748G 176Pin LQFP? There are none at the Freescale download-area...

 

Thank you in advance

Michael

Labels (1)
1 Solution
7,402 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It is attached in Reference manual.

Peter

View solution in original post

6 Replies
4,628 Views
royke
Contributor I

Hello

All links that can be found to this reference manual do not work. Hopefully someone can help with this reference manual

 

With kind regards 

0 Kudos
Reply
7,402 Views
PeterHartlmuell
Contributor I

Hi,

It is understood, that the signal description "is attached in Reference manual".

Nevertheless, I did not find any place to download this Excel file. Is it only available under an NDA?

Greetings, Peter

0 Kudos
Reply
7,402 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It is an embedded attachment in reference manual pdf format.

pastedImage_1.png

Please find in your pdf browser,viewer or editor the paperclip icon.

Under is are embedded attachment.

Peter

7,403 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It is attached in Reference manual.

Peter

7,402 Views
carlvanwormer
Contributor II

The attachment to the rev.5 reference manual document (IO_Signal_Description_and_Input_Multiplexing_Tables.xlsx) has errors in the pin names for both the 176LQFP and the BGA256 packages.  The rev.4 reference manual does not have these errors.  The bad names for 5 of the pins are all "#REF!", which is an Excel error for a bad cell reference.

7,402 Views
nathanimig
Contributor I

Hello, so I have been searching intrawebs for rev. 4 and I can't seem to find this anywhere. Is there anyway you could share this, it would be greatly appreciated?

0 Kudos
Reply