[MPC5748G] Optimize flash programming speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[MPC5748G] Optimize flash programming speed

1,167件の閲覧回数
BenMW
Contributor I

Hi, I want to know if anyone can tell me how to optimize the flash programming speed. Currently I'm using an OSJTAG adapter for progrmaming and debugging. Is there any recommendation for another adapter with higher speed? Or is it normal that it takes about 1,5 minutes to write the code into flash?

Here are my debug configuration settings:

BenMW_0-1639984212418.png

 

0 件の賞賛
返信
1 返信

1,154件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

The flashing time can be so, it also depends on number of P/E cycles (more times erased devices mean longer erase/program time).

Some debugger are capable re-flash only modified blocks (for instance Lauterbach TRACE32), in such case flash programming is mostly quite fast.

0 件の賞賛
返信