[MPC5748G] Optimize flash programming speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MPC5748G] Optimize flash programming speed

1,173 Views
BenMW
Contributor I

Hi, I want to know if anyone can tell me how to optimize the flash programming speed. Currently I'm using an OSJTAG adapter for progrmaming and debugging. Is there any recommendation for another adapter with higher speed? Or is it normal that it takes about 1,5 minutes to write the code into flash?

Here are my debug configuration settings:

BenMW_0-1639984212418.png

 

0 Kudos
Reply
1 Reply

1,160 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

The flashing time can be so, it also depends on number of P/E cycles (more times erased devices mean longer erase/program time).

Some debugger are capable re-flash only modified blocks (for instance Lauterbach TRACE32), in such case flash programming is mostly quite fast.

0 Kudos
Reply