MPC5744P: Example code for software full duplex UART using GPIO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744P: Example code for software full duplex UART using GPIO

2,350 次查看
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

 

does anyone have an idea where to find example code for a software UART (just using Rx and Tx) via GPIO pins?

Issue is that MPC5744P has only two LinFlex modules and in the application a third one is required for baudrates up to 115kbaud.

 

Thanks

 

br

Guenter

标签 (1)
0 项奖励
回复
2 回复数

1,687 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Here you can find an only example which is available for Panther UART at this time.

Example MPC5744P LINFlex UART echo SW polling

0 项奖励
回复

1,687 次查看
guenter_loettrich
NXP Employee
NXP Employee

Hi Peter,

thanks. I found that one as well. However I'm looking for a piece of software where a UART can be emulated using 2 GPIO pins and timers and probably DMA to create a third UART for the device. The application requires three UARTs but on Panther only two are realized in hardware.

br

Guenter

0 项奖励
回复