MPC5744P: Example code for software full duplex UART using GPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P: Example code for software full duplex UART using GPIO

2,420件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

 

does anyone have an idea where to find example code for a software UART (just using Rx and Tx) via GPIO pins?

Issue is that MPC5744P has only two LinFlex modules and in the application a third one is required for baudrates up to 115kbaud.

 

Thanks

 

br

Guenter

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,757件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Here you can find an only example which is available for Panther UART at this time.

Example MPC5744P LINFlex UART echo SW polling

0 件の賞賛
返信

1,757件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi Peter,

thanks. I found that one as well. However I'm looking for a piece of software where a UART can be emulated using 2 GPIO pins and timers and probably DMA to create a third UART for the device. The application requires three UARTs but on Panther only two are realized in hardware.

br

Guenter

0 件の賞賛
返信