MPC5741P How to create a linker for Code Flash blocks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5741P How to create a linker for Code Flash blocks

1,970 Views
tanveerahmed
Contributor I

@Hi ,

We are planning to use MPC5741P controller in our project. I went through the reference manual and found that memory block with below address

1. 0x010C0000 to 0x010FFFFF

2. 0x01140000 to 0x0117FFFF

3. 0x011C0000 to 0x011FFFFF

is not available for MPC5741P controller. But there are two blocks in between 0x01100000 to 0x0113FFFF and 0x01180000 to 0x011BFFFF which should be available for MPC5741P controller.

pastedImage_1.png

But i am finding it difficult how to create a linker file to include the blocks 0x01100000 to 0x0113FFFF and 0x01180000 to 0x011BFFFF as internal flash.

Can you please share any example for this use case.

Regards,

Tanveer

0 Kudos
Reply
2 Replies

1,814 Views
ybb34713
Contributor II

Have you solved the problem yet?

0 Kudos
Reply

1,814 Views
tanveerahmed
Contributor I

@David Tosenovjan can you please help for this topic.

0 Kudos
Reply